cancel
Showing results for 
Search instead for 
Did you mean: 

Can the evaluation board of the P-NUCLEO-IHM03 pack be used with expansion boards for controlling a stepper motor and brushed motors?

MKron.1
Associate

Hi

There is this motor control nucleo Pack P-NUCLEO-IHM03 which includes the NUCLEO-G431RB evaluation board, the X-NUCLEO-IHM16M1 expansion board and Gimbal motor GBM2804H-100T. I cannot find further information if the included evaluation board can be used with other expansion boards for motor control e.g. for brushed DC Motors.

Thank you for any help

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @MKron.1​, to the community!

The NUCLEO-G431RB included in the P-NUCLEO-IHM03 can of course also be used for other X-NUCLEO boards. For brushed DC motors, there is e.g. X-NUCLEO-IHM04A1 (based on L6206) or X-NUCLEO-IHM15A1 (based on STSPIN840).

However, the NUCLEO-G431RB came onto the market later, so the firmware for the above-mentioned X-NUCLEO still needs to be adapted, but this is possible in principle.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @MKron.1​, to the community!

The NUCLEO-G431RB included in the P-NUCLEO-IHM03 can of course also be used for other X-NUCLEO boards. For brushed DC motors, there is e.g. X-NUCLEO-IHM04A1 (based on L6206) or X-NUCLEO-IHM15A1 (based on STSPIN840).

However, the NUCLEO-G431RB came onto the market later, so the firmware for the above-mentioned X-NUCLEO still needs to be adapted, but this is possible in principle.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MKron.1
Associate

Thank you. Thats what I wanted know.