cancel
Showing results for 
Search instead for 
Did you mean: 

Can i use motor pilot with custom board

TKara.2
Associate III

I can use a motor profiler with a custom board, but can I use a motor pilot with the same software? Is it possible to use a motor pilot with a custom board?

 
 
1 ACCEPTED SOLUTION

Accepted Solutions
Gael A
ST Employee

Hello TKara.2,

Yes, it is possible to use the MotorPilot with a custom board as long as the Motor Control Protocol is enabled in the User Interface tab of the WorkBench.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.

View solution in original post

4 REPLIES 4
Gael A
ST Employee

Hello TKara.2,

Yes, it is possible to use the MotorPilot with a custom board as long as the Motor Control Protocol is enabled in the User Interface tab of the WorkBench.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.

Thanks @Gael A 

Hi, I'm trying to do the same with a custom made board, i've selected the "motor Control option/tab" in the MC workbench, however when trying to builed the project in IDE i get the following error:

J2Z69_0-1740047635757.png

How can i resolve this issue?

 

I'm using the STM32G431RBT6

This is because not all the necessary paths to the libraries were automatically added. Check the include path in the project settings.