2025-08-05 11:38 PM
Hello,
I used Motor Pilot v5.4.8 to identify and save the parameters of a motor. Then, using MCSDK v6.4, I created a project based on the same motor and the B-G431B-ESC1 board. I did not modify any settings or code during the project creation.
After generating the code and flashing it to the board using STM32CubeIDE, the motor did not start running as expected.
Then I opened Motor Pilot v6.4, connected to the board, and attempted to change the motor speed and start it — but I received an Overcurrent error immediately.
Here are my questions:
Why am I seeing an Overcurrent error when trying to start the motor, even though the parameters were previously identified and worked in v5.4.8?
Why is motor profiling no longer available in the new version of Motor Pilot (v6.4)? Has this feature been removed or moved elsewhere?
Any insights or suggestions would be greatly appreciated.
Thanks in advance!
2025-08-06 12:48 AM
Hello @AmirArsalan10,
Motor profiler is available in MCSDK6.4.0. Refer to the User Manual available through Workbench tool > About > Documentations > Documentation > User manual tab, and the Motor Profiler Application Note link.