2025-08-06 12:09 AM
Hello,
I’m a beginner working with STM32 and motor control. I want to learn how to:
Understand the code structure inside STM32CubeIDE
Flash the firmware to my board
Control the motor using Motor Pilot
To get started, I would like to know if there is a ready-to-use example project (source code) that I can open directly in STM32CubeIDE without having to generate it using MCSDK or MC Workbench.
Here are the details of my hardware setup:
Board: B-G431B-ESC1
Motor type: Permanent Magnet Synchronous Motor (PMSM)
Pole pairs: 20
If such a project exists, I would really appreciate it if you could share the source files or point me to an official ST example that matches this setup.
Thank you very much!