2024-07-30 2:08 AM
Hi,
I want to control BLDC motor with X-IHM07M1 motor driver and stm32 nucleo-G071RB microprocessor. I had read that this motor driver is compatible with Nucleo boards, but when I entered the Motor Control Workbench application, it only highlighted certain boards as options. After spending some time, I found and selected my board under the control unit section.
My question is, do I need to use one of the boards listed in the application for the motor driver to work ideally, or can I use my board without issues after selecting it as described?