cancel
Showing results for 
Search instead for 
Did you mean: 

Request MCSDK for Linux

test_dot
Associate

Please provide a Linux version of MCSDK. ST already has CubeMX and CubeIDE for Linux and they also run on Java, so I guess it should not be a problem.

Or even a better alternative, just provide source code for MCSDK examples in a git repository. It is very frustrating to obtain source code through CubeMX and always having to log in.

2 REPLIES 2
Simon
Associate III

Fully agree, there should be a linux version. People are moving away from Windows in droves so not having a linux version will hurt ST sales of the parts since we can't design with them.

Ozone
Principal III

I would agree.
There are plenty of portable or platform-independant GUI frameworks, so Linux versions should not require much effort.
While I don't have plans to use the MCSDK, I do all my projects for STM32s under Linux.