2024-04-16 12:58 AM - edited 2024-04-16 03:38 AM
Hi all, I have been trying to control my BLDC motor with an condition where if the surrounding temperature increases a threshold temperature the bldc motor should turn fast else slow. I am using lm35 as temperature sensor, i was able to interface this using stm32 nucleo g431rb board , esc and lm35 but i want to interface this through the code generated from motor control workbench. I need few insights on this, the code is generated for P-Nucleo-IHM03 motor control pack with FOC control algorithm.
2024-06-20 01:42 AM
Hello @hemanthgowdas,
As mentioned in MCSDK 6.3.0 post, a ST Motor Control Board Designer (STMCBD) tool is provided and gives to the users the ability to describe their own motor control hardware through an easy-to-use graphical interface. This description can then be used in the ST Motor Control Workbench.