2020-07-18 05:07 PM
I see in the schematic the potentiometer is referenced on pin 25, however I only see the PWM firmware setup example. Can someone point me to the correct setup?
Solved! Go to Solution.
2020-11-04 02:17 PM
Hello Laurent,
Yes, frustrating indeed since the potentiometer is already included on the PCB without an example to use it. As I mentioned in the thread months back I did try the other board examples with no success.
Please do let me know when I can exercise an example to complete tests that need to be done before moving forward in replacing another offering we use.
Best Regards,
--RW
2021-01-31 08:26 PM
Any good news?
2022-11-14 11:30 AM
Any good news?
2022-11-14 11:44 AM
Your the only response in 2 years...A couple weeks after my last request, I moved on to another non-st solution and that has been doing fine. Maybe someday they will update the ESC samples and I'll re-visit trying again on another project. Yeah, I felt abandoned and spent over $500 on ESC's and supporting items thinking it was going to be a slam dunk. Lesson learned, always have Plan B, C, D, etc. ready to go. 🙂