cancel
Showing results for 
Search instead for 
Did you mean: 

B-G431B-ESC1 potentiometer control

RWago.1
Associate II

I see in the schematic the potentiometer is referenced on pin 25, however I only see the PWM firmware setup example. Can someone point me to the correct setup?

13 REPLIES 13
RWago.1
Associate II

Hello Laurent,

Yes, frustrating indeed since the potentiometer is already included on the PCB without an example to use it. As I mentioned in the thread months back I did try the other board examples with no success.

Please do let me know when I can exercise an example to complete tests that need to be done before moving forward in replacing another offering we use.

Best Regards,

--RW

RWago.1
Associate II

Any good news?

KnarfB
Principal III

Any good news?

RWago.1
Associate II

Your the only response in 2 years...A couple weeks after my last request, I moved on to another non-st solution and that has been doing fine. Maybe someday they will update the ESC samples and I'll re-visit trying again on another project. Yeah, I felt abandoned and spent over $500 on ESC's and supporting items thinking it was going to be a slam dunk. Lesson learned, always have Plan B, C, D, etc. ready to go. 🙂