2024-12-15 03:47 PM
Hi ST Team,
Unfortunately, I faced an error of "Port Open and try to configure the board and I'm stuck here. It's a very similar problem with this discussion :
and also heavily influenced on setting up through this youtube video :
https://www.youtube.com/watch?v=KHFnd9NY0S0
What I have done :
-. Please find my wiring on the photo attached.
-. So I have already connected the V+ and V- (3S Voltage - I'm interested in) to a power supply and also the PWM and GND to an external microcontroller (an Arduino setup generating 490Hz PWM).
-. Micro USB connected to my PC, also have updated the FW on STLINK Utility.
-. Flash the B-G431B-ESC1 firmware through the STM32CubeProgrammer.
-. PORT can be successfully opened with 115200 baud rate
I'm assuming the ESC is as easy as setting them up like that and Motor Pilot will just start profiling my motor, but am I still missing something of configuring the board?