Hi @hellouniverse,I see. What parameters did you use on that video? It seems like you're limited to 0.5A. Do you have anything that would limit you to this value?Also, could you give me the actual motor reference that you are using? In your screensho...
Hi @hellouniverse,First of all, I see 1A on your power supply photo. Are you sure you are not hitting the Over Current Protection (OCP) value of your power supply?Your problem seems to be firmware related. Can you tell which firmware you are using fo...
Hi @TNaum,I apologize for the oversight. It seems the hal_RTC.c files were unintentionally linked to my MX repository.I'm sending you a new project, which I have tested on another computer to ensure it works correctly. In this example code, LD2 shoul...
Hi @yassir,Can you give more details about the board you are using?By default, you cannot see if the CPU is in sleep mode or not just from the pins. You would need to do some config first. Still, the quickest way would be to measure IDD and compare i...
Hi @TNaum,I fixed the code that contained local references. I recommend opening it with CubeIDE.Please tell me if you have any trouble running it.About the power consumption, I am using a power shield on the VDD selection pin (JP5). So the measured 3...