2024-03-18 8:54 AM
To whom it may concern,
I am developing a controller for BLDC, I managed to initialize the board with cubeIDE and flash code (so far only turning on the LED).
However, I need to use a BLDC motor for my project and I have searched everywhere on how to initialize and do a motor profiler, etc. But there is no information about how it works, just that it doesn't.
Could you please provide information on how to set up the 6-step controller with b-g431b-esc1 and which software should be used, since so far none of your released software works.
This is the BLDC motor I am using: https://maytech.cn/products/mto5065-170-ha-c
Any help would be appreciated.
Sincerely,
Mykolas
2024-03-19 6:25 AM
Hello,
Please use STM32 Motor Control Software Development Kit tool.
User manual UM3027 How to use STM32 motor control SDK v6.0 workbench available here.