2023-12-08 10:00 AM - edited 2023-12-08 11:42 AM
Squeeling starts, right around 2KRPM:
Solved! Go to Solution.
2023-12-13 11:33 PM
Glad to hear that you managed to get through it.
1. That's in fact a feature (open loop mode) currently missing but that will become available soon in the next release
2. I see you are using a wrong interface (the FOC one). You can load the 6step interface of the MotorPilot by clicking "GUI" in the upper bar, then "Load GUI". You have to select the "MC_6STEP_SDK.qml" file in the installation folder (that in my case was "C:\Program Files (x86)\STMicroelectronics\MC_SDK_6.2.0\Utilities\PC_Software\STMotorPilot\GUI"). You can get all the updated documentation on the web page Web page documentation or in Motor Control wiki wiki_Motor_Control
3. To avoid the conflict between MCU resources, select a different timer for the speed controller in the workbench (tab "Speed sensing config", for instance TIM4)