Skip to main content
Associate
November 20, 2024
Question

Error: X509 - Signature Algorithm (OID) is Unsupported in mbed TLS 2.16.2 During Azure MQTT Connection

  • November 20, 2024
  • 1 reply
  • 1093 views

I’m currently using mbed TLS 2.16.2 on an STM32F407G microcontroller with a SIM7600G GSM module to connect to an Azure MQTT broker over a GSM network. During the certificate parsing, I’m encountering the following error:

"X509 - Signature algorithm (oid) is unsupported : OID - OID is not found"

 

  • The STM32F407G is successfully initialized and connected to the GSM network via the SIM7600G.
  • The device obtains an IP address and the connection to the Azure MQTT broker is established.
  • However, when mbed TLS tries to parse the root certificate, it fails due to an unsupported or unrecognized signature algorithm in the certificate.

 

 

  • I’ve ensured that mbed TLS has the correct configuration options enabled for RSA and SHA256 support in config.h (such as #define MBEDTLS_RSA_C, #define MBEDTLS_X509_RSASSA_PKCS1_V1_5, and #define MBEDTLS_SHA256_C).
  • The broker’s certificate is from a trusted authority (DigiCert Global Root G2).
  • I’ve checked if mbed TLS supports the signature algorithm used by the certificate but haven’t had any luck resolving the issue.

 

const char mbedtls_root_certificate[] = "-----BEGIN CERTIFICATE-----\r\n"
 "MIIDjjCCAnagAwIBAgIQAzrx5qcRqaC7KGSxHQn65TANBgkqhkiG9w0BAQsFADBh\r\n"
 "MQswCQYDVQQGEwJVUzEVMBMGA1UEChMMRGlnaUNlcnQgSW5jMRkwFwYDVQQLExB3\r\n"
 "d3cuZGlnaWNlcnQuY29tMSAwHgYDVQQDExdEaWdpQ2VydCBHbG9iYWwgUm9vdCBH\r\n"
 "MjAeFw0xMzA4MDExMjAwMDBaFw0zODAxMTUxMjAwMDBaMGExCzAJBgNVBAYTAlVT\r\n"
 "MRUwEwYDVQQKEwxEaWdpQ2VydCBJbmMxGTAXBgNVBAsTEHd3dy5kaWdpY2VydC5j\r\n"
 "b20xIDAeBgNVBAMTF0RpZ2lDZXJ0IEdsb2JhbCBSb290IEcyMIIBIjANBgkqhkiG\r\n"
 "9w0BAQEFAAOCAQ8AMIIBCgKCAQEAuzfNNNx7a8myaJCtSnX/RrohCgiN9RlUyfuI\r\n"
 "2/Ou8jqJkTx65qsGGmvPrC3oXgkkRLpimn7Wo6h+4FR1IAWsULecYxpsMNzaHxmx\r\n"
 "1x7e/dfgy5SDN67sH0NO3Xss0r0upS/kqbitOtSZpLYl6ZtrAGCSYP9PIUkY92eQ\r\n"
 "q2EGnI/yuum06ZIya7XzV+hdG82MHauVBJVJ8zUtluNJbd134/tJS7SsVQepj5Wz\r\n"
 "tCO7TG1F8PapspUwtP1MVYwnSlcUfIKdzXOS0xZKBgyMUNGPHgm+F6HmIcr9g+UQ\r\n"
 "vIOlCsRnKPZzFBQ9RnbDhxSJITRNrw9FDKZJobq7nMWxM4MphQIDAQABo0IwQDAP\r\n"
 "BgNVHRMBAf8EBTADAQH/MA4GA1UdDwEB/wQEAwIBhjAdBgNVHQ4EFgQUTiJUIBiV\r\n"
 "5uNu5g/6+rkS7QYXjzkwDQYJKoZIhvcNAQELBQADggEBAGBnKJRvDkhj6zHd6mcY\r\n"
 "1Yl9PMWLSn/pvtsrF9+wX3N3KjITOYFnQoQj8kVnNeyIv/iPsGEMNKSuIEyExtv4\r\n"
 "NeF22d+mQrvHRAiGfzZ0JFrabA0UWTW98kndth/Jsw1HKj2ZL7tcu7XUIOGZX1NG\r\n"
 "Fdtom/DzMNU+MeKNhJ7jitralj41E6Vf8PlwUHBHQRFXGU7Aj64GxJUTFy8bJZ91\r\n"
 "8rGOmaFvE7FBcf6IKshPECBV1/MUReXgRPTqh5Uykw7+U0b6LJ3/iyK5S9kJRaTe\r\n"
 "pLiaWN0bfVKfjllDiIGknibVb63dDcY3fe0Dkhvld1927jyNxF1WW6LZZm6zNTfl\r\n"
 "MrY=\r\n"
 "-----END CERTIFICATE-----\r\n";

// Define the length of the certificate
const size_t mbedtls_root_certificate_len = sizeof(mbedtls_root_certificate);



mbedtls_x509_crt cert;
 mbedtls_x509_crt_init(&cert);

 char error_buf[100];
 ret = mbedtls_x509_crt_parse(&cert, (const unsigned char *)mbedtls_root_certificate, mbedtls_root_certificate_len+1);
 if (ret != 0) {
 mbedtls_strerror(ret, error_buf, sizeof(error_buf));
 printf("Failed to parse root certificate: %s\n", error_buf);
 char oid_buf[32];
 mbedtls_oid_get_numeric_string(oid_buf, sizeof(oid_buf), &cert.sig_oid);
 printf("Signature Algorithm: %s\n", oid_buf);
 } else {
 printf("Root certificate parsed successfully.\n");
 }​

 

 

  1. Is there a specific mbed TLS configuration option I might be missing to support this certificate’s signature algorithm?
  2. Does the error point to a version issue with mbed TLS? If so, would updating to a newer version solve the problem?
  3. Is there a way to debug or inspect the OID of the certificate’s signature algorithm to understand why it’s not recognized?

Any guidance or suggestions would be greatly appreciated!

 

 

 

This topic has been closed for replies.

1 reply

Visitor II
November 20, 2024

Use tools like OpenSSL to inspect the certificate:

 

 

openssl x509 -in root_certificate.pem -text -noout