STM32 MCUs Machine learning & AI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Edge AI for all. NanoEdge AI Studio autoML tool, now free for STM32 and open to all ARM Cortex-M bas

NanoEdge AI Studio v4.3 is now offered for free to all engineers, giving them the opportunity to create highly efficient TinyML libraries that can be deployed on Cortex-M based microcontrollers. In addition, other enhancements have been integrated to...

ST30449_nanoedge-ai-studio-motor (2).jpg ST30449_nanoedge-ai-studio-motor (2).jpg

Object detection - STM32H747i-disco

Hi,I'm trying to implement a detection model on a STM32-H747i-disco board, the only example provided is the one called "people counting", but the libraries are provided in binary format and it seems that it is not possible to modify them. How could w...

R.SOLER by Associate
  • 522 Views
  • 2 replies
  • 0 kudos

I am having an issue in the code generated from X-CUBE-AI library. The C generated code for my tflite model (called network) is giving following error: /X-CUBE-AI/App/network.h:40:3: error: invalid initializer

The error is in the network.c code file generated by the X-CUBE-AI library. I have chosen "Not Selected" option in drop down option for X-CUBE-AI. The code below is giving the error as mentioned:

0693W00000bhR9nQAE.png
BFaru.1 by Associate II
  • 357 Views
  • 2 replies
  • 0 kudos