2021-01-28 02:03 AM
I am working with the STM32F769 microcontroller and it's using FreeRTOS operating system. It uses the following clock configuration (216 MHz SystemCoreClock):
/** System Clock Configuration
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/**Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN = 432;
RCC_OscInitStruct.PLL.PLLQ = 9;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLR = 2; /* Even when DSI is disabled PLLR with 2 <= PLLR <= 7 according to RM0410 p.163 */
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Activate the Over-Drive mode
*/
if (HAL_PWREx_EnableOverDrive() != HAL_OK)
{
Error_Handler();
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
{
Error_Handler();
}
I have written a software transmit-only UART running at 3 MBaud on any arbitrary GPIO pin. For the most part it works great, but every once in a while, especially in interrupts, it starts "writing in Chinese" and strange characters appear in my terminal window. Does anybody know what's wrong?
#define IDLE_STATE 1
#define DISABLE_ALL_INTS_IF_NECESSARY() uint32_t old_primask; \
old_primask = __get_PRIMASK(); \
__disable_irq()
#define ENABLE_ALL_INTS_IF_THEY_WERE_ENABLED() if (!old_primask) \
{ \
__enable_irq(); \
}
static GPIO_TypeDef* TxPort_;
static uint16_t TxPin_;
void LL_UART_SW_TxOnly_enable(GPIO_TypeDef* TxPort, uint16_t TxPin) {
TxPort_ = TxPort;
TxPin_ = TxPin;
GPIO_InitTypeDef initStruct = {TxPin_, GPIO_MODE_OUTPUT_PP, GPIO_NOPULL, GPIO_SPEED_LOW, 0};
HAL_GPIO_Init(TxPort_, &initStruct);
SET_PIN(TxPort_, TxPin_, IDLE_STATE);
}
void LL_UART_SW_TxOnly_disable(void) {
GPIO_InitTypeDef initStruct = {TxPin_, GPIO_MODE_ANALOG, GPIO_NOPULL, GPIO_SPEED_LOW, 0};
HAL_GPIO_Init(TxPort_, &initStruct);
}
/* 216 MHz system clock */
#define OUTPUT_BIT(__BIT_NO__) *BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__]; \
*BSRR = BSRRvalues[__BIT_NO__];
inline static void __attribute__((optimize("O0"))) outputByte(volatile uint32_t* BSRR, uint32_t BSRRvalues[10]) {
OUTPUT_BIT(0);
OUTPUT_BIT(1);
OUTPUT_BIT(2);
OUTPUT_BIT(3);
OUTPUT_BIT(4);
OUTPUT_BIT(5);
OUTPUT_BIT(6);
OUTPUT_BIT(7);
OUTPUT_BIT(8);
*BSRR = BSRRvalues[9];
}
// Superfast (3 MBit/s) UART
void __attribute__((optimize("O3"))) LL_UART_SW_TxOnly_transmitByte(uint8_t byteToSend) {
uint32_t BSRRvalues[10];
BSRRvalues[0] = (IDLE_STATE == 1) ? (((uint32_t)TxPin_) << 16) : TxPin_; // Start bit
BSRRvalues[9] = (IDLE_STATE == 0) ? (((uint32_t)TxPin_) << 16) : TxPin_; // Stop bit
BSRRvalues[1] = BSRRvalues[(byteToSend & 0x01) ? 9 : 0]; // Bit 0
BSRRvalues[2] = BSRRvalues[(byteToSend & 0x02) ? 9 : 0]; // Bit 1
BSRRvalues[3] = BSRRvalues[(byteToSend & 0x04) ? 9 : 0]; // Bit 2
BSRRvalues[4] = BSRRvalues[(byteToSend & 0x08) ? 9 : 0]; // Bit 3
BSRRvalues[5] = BSRRvalues[(byteToSend & 0x10) ? 9 : 0]; // Bit 4
BSRRvalues[6] = BSRRvalues[(byteToSend & 0x20) ? 9 : 0]; // Bit 5
BSRRvalues[7] = BSRRvalues[(byteToSend & 0x40) ? 9 : 0]; // Bit 6
BSRRvalues[8] = BSRRvalues[(byteToSend & 0x80) ? 9 : 0]; // Bit 7
DISABLE_ALL_INTS_IF_NECESSARY();
outputByte(&TxPort_->BSRR, BSRRvalues);
ENABLE_ALL_INTS_IF_THEY_WERE_ENABLED();
}
void LL_UART_SW_TxOnly_transmitBuffer(uint8_t* pData, uint16_t numBytes) {
while (0 < numBytes--) {
LL_UART_SW_TxOnly_transmitByte(*pData++);
}
}
void LL_UART_SW_TxOnly_transmitNullTermString(const char* pData) {
while (*pData != 0) {
LL_UART_SW_TxOnly_transmitByte(*pData++);
}
}
2021-01-29 12:22 PM
The NOP can even not happen at all!
NOP does nothing. NOP is not necessarily a time-consuming NOP. The processor might remove it from the pipeline before it reaches the execution stage.
Use NOP for padding, for example to place the following instruction on a 64-bit boundary.
2021-01-29 12:47 PM
Both SysTick and DWT counters are local to CPU core and could be used with appropriate code. Though DWT could be easier as it's 32-bit. Still GPIO on AHB with polling some timer on APB also should be good enough.
Take a look on SEGGER RTT, J-Scope and SystemView. 😉
https://www.segger.com/products/debug-probes/j-link/technology/about-real-time-transfer/
https://www.segger.com/products/debug-probes/j-link/tools/j-scope/
https://www.segger.com/products/development-tools/systemview/
2021-01-29 01:41 PM
DSB is often used as a time-wasting instruction instead of NOP.
What's wrong with using hardware UARTs? Yes, there's limitation on which pins you can use them, and yes, there are only 8 of them in the 'F769; but OTOH they tend to work properly all the time.
JW
2021-01-29 01:57 PM
If its TX only you could try 10-bit SPI transfers and ignore the clock pin.
2021-01-30 11:14 AM
> What's wrong with using hardware UARTs?
We have 10 microcontrollers on the PCB, all are ball grid arrays and all of them have hardware UART:s. On 9 of them we have filters that degrade the signals at high frequencies so we can't go any faster than 115200. The 10th microcontroller has trace implemented and I tried it once and never would I touch that again, not even with a polestick. So, if I want fast logging (highspeed buses are difficult to debug with a 115200 UART) without making another spin of the PCB, the only option left it to try to find nets that appear on pad/vias and can double-function as UART as well and then solder wires onto them.
2021-01-30 01:09 PM
Or, if you have 2 lines available, you can try to bitbang SPI.
Btw on a development board, I'd simply remove the filters.
JW
2021-01-30 07:24 PM
I sure wouldn't want to bit-bang at 3-megabaud !
2021-01-31 12:13 AM
> I sure wouldn't want to bit-bang at 3-megabaud !
Next week I'm planning to order 12 MBaud cables ( https://ftdichip.com/products/c232hd-ddhsp-0 ). Btw, does anybody know if there are even faster cables available on the market?
2021-02-01 03:21 AM
DSB worked great! Btw, I read your great website, lots of very helpful information! But now I'm afraid to program STM32 microcontrollers, now that I know how much complexity there is "under the surface"...
2021-02-01 03:26 AM
Have a look at orbuculum https://github.com/orbcode/orbuculum and the help you can get from Mubes on the discord orbuculum channel before you dump SWO/Trace.