cancel
Showing results for 
Search instead for 
Did you mean: 

Using STM32 examples on custom boards

dryet
Associate II

Hello,

I have made a custom board using the STM32WB55CEU6 chip and I would like to try out some examples that are available from ST. My problem is that these examples are made for STM32WB55CG and I can't find an easy way to change target of these examples. In the read me file it says:

This example has been tested with NUCLEO-G431KB RevA board and can be

easily tailored to any other supported device and development board.

But i can't seem to find an easy way to do it. 

My current aproach is:

- Getting the example project using CubeMX.

- Creating new project with the desired target

- Importing .ioc project configuration

After that I have the same configuration but the project is obviously empty. The example files are linked so i can't copy them. 

Thank you in advance for any help.

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @dryet ,

I recommend you follow this FAQ: MCU1 to MCU2 migration option within STM32CubeIDE.

You can also refer to the Tutorial 5: "Exporting current project configuration to a compatible MCU" in UM1718.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

1 REPLY 1
Imen.D
ST Employee

Hello @dryet ,

I recommend you follow this FAQ: MCU1 to MCU2 migration option within STM32CubeIDE.

You can also refer to the Tutorial 5: "Exporting current project configuration to a compatible MCU" in UM1718.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen