cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L452 current consumption in STOP 2 mode is less than datasheet indications.

Jsine.1
Associate II

When I run the PWR_STOP2 example from the STM32Cube_FW_L4_V1.15.0 on a STM32L452VE, I measure a current consumption egal to 1.6 uA instead of 2.05 uA.

The datasheet and STM32CubeMX indicate 2.05 uA without RTC for this target.

It's a great news 8) but I'm afraid that it hides something wrong.

For information, when I run this same example for and on a STM32L476, the current measured is in accordance to the datasheet indications.

Can you help to understand this good news? ;)

In advance, thank you.

5 REPLIES 5
Uwe Bonnes
Principal III

Datasheet value may differ from the typical values but not be more tha the max value, if given.

You ambient temperature may also differ, having also great influence.

Jsine.1
Associate II

Thank you.

My ambient temperature is about 25°C.

With STM32CubeMX, the current consumption simulation doesn't allow to have a consumption less than 2.05 uA in STOP 2 mode.

Often, the values indicate are the best that we hope to observe. Is it right?

Uwe Bonnes
Principal III

Typical values are typical. About 50 % of parts will be above and 50 % below that value.

Jsine.1
Associate II

Even for a low power consumption?

Uwe Bonnes
Principal III

Yes. That is what typical values are for.