2019-05-03 06:28 AM
Solved! Go to Solution.
2019-06-12 05:51 AM
Hi @MMagl ,
I am coming back to answer your question.
The current STM32H7 bootloader doesn't support CAN interface. The AN2606 is the reference and is the correct one.
However, for STM32H7 rev V devices, the FDCAN bootloader interface will be supported.
AN2606, AN4938 and AN3154 will be updated accordingly.
-AMel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-05-03 06:47 AM
It seems that STM forum have some restriction for text formatting and I end-up with strange post. Here is my second attempt.
Can I perform boot via CAN interface using the STM32H750 boot loader?
According to AN4938 page 24 chapter 5.3 says that CAN2 PB5/PB13 can be used for boot.
That is why I asking this question
Thanks in advance
2019-06-12 05:51 AM
Hi @MMagl ,
I am coming back to answer your question.
The current STM32H7 bootloader doesn't support CAN interface. The AN2606 is the reference and is the correct one.
However, for STM32H7 rev V devices, the FDCAN bootloader interface will be supported.
AN2606, AN4938 and AN3154 will be updated accordingly.
-AMel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-06-12 06:14 AM
Thanks for clarification
The message thread can be put to solved state
Thanks,
Mirtcho