cancel
Showing results for 
Search instead for 
Did you mean: 

External loader for STM32H750 discovery

Andrew_Ghaly
Associate

Hi,

I am searching for the external loader to flash the h750 discovery board. Can you please help me?

Best regards,

Andrew

2 REPLIES 2
KDJEM.1
ST Employee

Hello @Andrew_Ghaly, and welcome to the community,

 

Are you looking for the MTFC4GACAJCN_STM32H750B-DISCO.stdlr and MT25TL01G_STM32H750B-DISCO.stdlr files?

You'll find these files after installing STM32CubeProgrammer under the installation folder ..\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoader

KDJEM1_0-1740668460942.png

Also, you can used STM32cubeProgrammer to select these external loader.

KDJEM1_1-1740668699183.png

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

MNema.1
Associate III

When I use this loader I always get errors if I check verification though. 
I mean MTFC4GACAJCN_STM32H750B-DISCO