STM32H743VIT6 can't connect with a LAN8720!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-21 4:55 AM
I have WeAct STM32H743 (STM32H743VIT6 ) and I can't connect it with a LAN8720 module!
I did all my steps according by example from this link https://www.st.com/en/embedded-software/stm32cubeh7.html
But, it doesn't help me!
How to find out at what stage I have break a code?
- Labels:
-
Ethernet
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-24 12:41 PM
Did you try this https://community.st.com/s/article/How-to-create-project-for-STM32H7-with-Ethernet-and-LwIP-stack-working
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-24 12:54 PM
Thanks for the answer!
Unfortunately I only have the ability to connect only RMII mode. Do you have the same detailed instruction but for RMII Mode?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-25 4:59 PM
Hello, No idea from your writing what happen nor issue type to try help you.
At first are you using a custom board? How did you connected PHY 8720 to board?
Is some way software running or terminate with hard fault?
8720 is an RMII only device like the 8742, this need change PHY driver. Browse forum, you can find driver and instruction to patch software.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-09-21 3:29 PM
Hi DK.
Did you ever sort this out?
I have exactly the same problem. I've tried the the LAN8720 and DP83848. with no luck.
I've tried it on the WeAct STM32H743 and the WeAct STM32H723. I've spent several days on this so far - and I've tried absolutley everything I can think of.
I have tried the LAN8720 and DP83848 on modified nucleo boards (the H743ZI) and they both work fine -
Note the LAN8720 is dropping packets on the Nucleo, but the LAN8720 isn't compatable with the H7, because of timing issues - there is a post on this somewhere - this is why the LAN8720 isn't in the HAL for the H7. But apart from dropped packets it works with ping 80% (on the Nucleo). The DP83848 is rock solid.
thanks
Mark
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-09-22 10:20 PM
So you have the MDIO working and "talk" to the PHY?
I had a retransmission problem when PHY was connected in full duplex, but STM32 worked in half-duplex because of reading the wrong PHY register / bit concerning auto-negotiation / success.