cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743iiK6 project with SD card not working

SK52
Associate

Hi,

   I worked for last three weeks STM32H743iik6 project with SD card .SD card with SPI interface but I got FR_NOT_READY error.I have checked hardware connection.same code work in stm32f and stm32 l series.I don't know reason for stm32h series not working.please any one have code stm32h series please send me.

 

 

 

2 REPLIES 2
Danish1
Lead III

Stm32h7xx is very different from stm32f4 and stm32l, in that it uses many more caches and other performance-enhancing techniques. Unless you add things like __dsb() and cache-related code where necessary (I explicitly disable cacheing in memory-regions where I use DMA, but ST seem to favour explicit flushing/invalidating before/after DMA) you are likely to hit problems.

This is a bit of a long-shot. What revision is your stm32h743?

Years ago I started a project around a stm32h743 (actually trying to port from a board that took stm32f767 because I wanted more RAM). But I have up after struggling for a long time with the SD-card interface. This was with stm32h743 Revision Y, which has loads of errata to do with its sdmmc peripheral.

I have recently revisited the project using the newer Revision V that has many of the sdmmc errata fixed. The sdmmc bit currently works (based on HAL; I am not a fan of HAL and I intend to rewrite the code when I get the opportunity).

Hello @SK52  

Please refer to the example Projects/STM32H743I-EVAL/Examples/SD in the STM32CubeH7 firmware as a starting point for your application.

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar