2024-05-01 12:11 AM - edited 2024-05-01 4:21 AM
Hi, I'm using a timer to create a software delay on a high prio task (HPTask with FreeRTOS).
The MCU used is STM32H755ZI.
My target is:
To reach this result I used TIM17 and OnePulse API.
This is my setup on main from CubeMX:
htim17.Instance = TIM17;
htim17.Init.Prescaler = 200;
htim17.Init.CounterMode = TIM_COUNTERMODE_UP;
htim17.Init.Period = 10000;
htim17.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim17.Init.RepetitionCounter = 0;
htim17.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim17) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_OnePulse_Init(&htim17, TIM_OPMODE_SINGLE) != HAL_OK)
{
Error_Handler();
}
This is my setup to generate the delay:
HAL_TIM_Base_Init(&htim17);
HAL_TIM_Base_Start_IT(&htim17);
HAL_TIM_OnePulse_Start(&htim17, 0U);
Now... I reached something that is usable but not exactly what I want.
The interrupt receives two events. Before to start and at the end of the pulse.
Is it possible (also adopting different strategies) to get only on single interrupt at the end of the period?
Thank you in advance,
C.
Solved! Go to Solution.
2024-05-05 11:13 PM
My mistake, lack of knowledge on this framework...
Remove the OnePulse setup and start.
2024-05-05 11:13 PM
My mistake, lack of knowledge on this framework...
Remove the OnePulse setup and start.