stm32g0b1ke mcu i2c not detected after flashing into flash memory
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-08-11 6:07 AM
I have flashed the firmware into flash memory using i2c application programming.when the controller is booting from flash memory,i can see the uart console logs .
I have configured the PB6 and PB7 pins are i2c pins.I set the clock speed to fast mode using stm32cubemx generator.I2c own address bit also set with 7bit I2C address << 1.But i2c is not detected.Is there any configuration missing?
Labels:
- Labels:
-
Bootloader
-
I2C
-
STM32G0 Series
0 REPLIES 0