STM32F767 + CMSIS DSP + Keil = Error.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-27 2:08 PM
Im trying to use rftt_q15 from CMSIS DSP libraries on my STM32F767Zi
The following error I get is quite strange. it says
#error "Define according the used Cortex core ARM_MATH_CM7, ARM_MATH_CM4, ARM_MATH_CM3, ARM_MATH_CM0PLUS, ARM_MATH_CM0, ARM_MATH_ARMV8MBL, ARM_MATH_ARMV8MML"
which is called from this:
#if defined(ARM_MATH_CM7)
#include "core_cm7.h"
#define ARM_MATH_DSP
#elif defined (ARM_MATH_CM4)
#include "core_cm4.h"
#define ARM_MATH_DSP
#elif defined (ARM_MATH_CM3)
#include "core_cm3.h"
#elif defined (ARM_MATH_CM0)
#include "core_cm0.h"
#define ARM_MATH_CM0_FAMILY
#elif defined (ARM_MATH_CM0PLUS)
#include "core_cm0plus.h"
#define ARM_MATH_CM0_FAMILY
#elif defined (ARM_MATH_ARMV8MBL)
#include "core_armv8mbl.h"
#define ARM_MATH_CM0_FAMILY
#elif defined (ARM_MATH_ARMV8MML)
#include "core_armv8mml.h"
#if (defined (__DSP_PRESENT) && (__DSP_PRESENT == 1))
#define ARM_MATH_DSP
#endif
#else
#error "Define according the used Cortex core ARM_MATH_CM7, ARM_MATH_CM4, ARM_MATH_CM3, ARM_MATH_CM0PLUS, ARM_MATH_CM0, ARM_MATH_ARMV8MBL, ARM_MATH_ARMV8MML"
#endif
However I have defined in main:
#define ARM_MATH_CM7;
then I removed this code and did what it would do if it saw ARM_MATH_CM7
#include "core_cm7.h" but if gave 35 errors saying that:
..\Drivers\CMSIS\DSP\Include\arm_math.h(5791): error: #757: function "int32_t" is not a type name
and other funny things like that
I have added include and source paths and also Included them from Keil project window
any ideas???
Solved! Go to Solution.
- Labels:
-
CMSIS
-
DSP
-
STM32F7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-27 2:21 PM
>>However I have defined in main: #define ARM_MATH_CM7;
Normally you'd put it in the compiler's command line define list, and without semicolons
ARM_MATH_CM7
__FPU_PRESENT=1U
I'd expect stm32f7xx_hal.h to define uint32_t
otherwise stdint.h
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
‎2020-08-27 2:21 PM
>>However I have defined in main: #define ARM_MATH_CM7;
Normally you'd put it in the compiler's command line define list, and without semicolons
ARM_MATH_CM7
__FPU_PRESENT=1U
I'd expect stm32f7xx_hal.h to define uint32_t
otherwise stdint.h
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
‎2020-08-27 2:51 PM
Thank you Clive or your response
I am a little bit confused however
I am guessing I didn't specify it in a correct place.
where exactly do I need to write that down?
Do I need to add something to the blue circle related to CMSIS or do I leave it as it is
again, thanks for your response
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-09 4:34 AM
Hi @hashtala​ ,
If you didn't yet found the answer to your question: the new defines need to appear in "Preprocessor Symbols" section.
Look to the configuration used in the project STM32CubeExpansion_AN4667_F7_V4.0.0\Projects\STM32F769I_EVAL\stm32f7_performances for example:
This example with some other ones are available in the package X-CUBE-32F7PERF.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-09 3:05 PM
Thanks Amel
I got it up and running smoothly but do not remember how exactly I solved it
I think I just added definition of __FPU_PRESENT somewhere in my code instead
Thanks for the solution