2025-07-29 8:49 AM
“I have already #include "arm_math.h" and added the DSP library in CubeMX, so why am I still getting the following errors: undefined reference to 'arm_cfft_init_f32', undefined reference to 'arm_cfft_f32', undefined reference to 'arm_cmplx_mag_f32'?”
"Here is the CMakeLists.txt file generated by CubeMX."
cmake_minimum_required(VERSION 3.22)
# Enable CMake support for ASM and C languages
enable_language(C ASM)
# STM32CubeMX generated symbols (macros)
set(MX_Defines_Syms
USE_PWR_LDO_SUPPLY
USE_HAL_DRIVER
STM32H723xx
$<$<CONFIG:Debug>:DEBUG>
)
# STM32CubeMX generated include paths
set(MX_Include_Dirs
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Inc
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Inc
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/CMSIS/Device/ST/STM32H7xx/Include
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/CMSIS/Include
${CMAKE_CURRENT_SOURCE_DIR}/../../Middlewares/ST/ARM/DSP/Inc
)
# STM32CubeMX generated application sources
set(MX_Application_Src
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/main.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/gpio.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/adc.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/dac.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/dma.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/usart.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/tim.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/stm32h7xx_it.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/stm32h7xx_hal_msp.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/sysmem.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/syscalls.c
${CMAKE_CURRENT_SOURCE_DIR}/../../startup_stm32h723xx.s
)
# STM32 HAL/LL Drivers
set(STM32_Drivers_Src
${CMAKE_CURRENT_SOURCE_DIR}/../../Core/Src/system_stm32h7xx.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_adc.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_adc_ex.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc_ex.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash_ex.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_gpio.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_hsem.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dma.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dma_ex.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_mdma.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pwr.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pwr_ex.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_cortex.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_i2c.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_i2c_ex.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_exti.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dac.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dac_ex.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_uart.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_uart_ex.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim.c
${CMAKE_CURRENT_SOURCE_DIR}/../../Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim_ex.c
)
# Drivers Midllewares
# Link directories setup
set(MX_LINK_DIRS
)
# Project static libraries
set(MX_LINK_LIBS
STM32_Drivers
${TOOLCHAIN_LINK_LIBRARIES}
)
# Interface library for includes and symbols
add_library(stm32cubemx INTERFACE)
target_include_directories(stm32cubemx INTERFACE ${MX_Include_Dirs})
target_compile_definitions(stm32cubemx INTERFACE ${MX_Defines_Syms})
# Create STM32_Drivers static library
add_library(STM32_Drivers OBJECT)
target_sources(STM32_Drivers PRIVATE ${STM32_Drivers_Src})
target_link_libraries(STM32_Drivers PUBLIC stm32cubemx)
# Add STM32CubeMX generated application sources to the project
target_sources(${CMAKE_PROJECT_NAME} PRIVATE ${MX_Application_Src})
# Link directories setup
target_link_directories(${CMAKE_PROJECT_NAME} PRIVATE ${MX_LINK_DIRS})
# Add libraries to the project
target_link_libraries(${CMAKE_PROJECT_NAME} ${MX_LINK_LIBS})
# Add the map file to the list of files to be removed with 'clean' target
set_target_properties(${CMAKE_PROJECT_NAME} PROPERTIES ADDITIONAL_CLEAN_FILES ${CMAKE_PROJECT_NAME}.map)
# Validate that STM32CubeMX code is compatible with C standard
if((CMAKE_C_STANDARD EQUAL 90) OR (CMAKE_C_STANDARD EQUAL 99))
message(ERROR "Generated code requires C11 or higher")
endif()
2025-07-30 10:58 PM
Unclear issue to me, please could you give us more details ?
Is it a build (compile / link steps) issue or code indexing (editor report) issue ?
Another post here if helping : https://community.st.com/t5/stm32-mcus-products/arm-bitreversal-32-undefined-reference-in-cmsis-dsp/td-p/383155
2025-07-30 11:47 PM
I think it should be a problem with compiling links
2025-08-01 1:03 PM
Hi @smile ,
I couldn't spot the missing functions in your attachment so I'm not sure why you provided that.
Anyway, you just need to search your project for the missing symbols, if they're not present that's your problem. If they are present, then you need to check that paths to the sieve files are in your project's source paths. If the relevant sources are compiling but failing to link then you need to check the project link config.