2025-02-04 10:18 PM - edited 2025-02-07 3:09 AM
I am using CUBEMX Version 6.10
STMCUBE IDE 1.16.0
FW version F7V1.17.0
Enabled LWIP ETH With FREERTOS CMSIS2
same settings did with cmsis version 1 it's working but with cmsis version2 NOT Working
I configured on internal Timer TIM1
as soon as I connect Eth Cable program counter not reaching threads & Timer callback / TIM6(systick update).
I checked in fault handlers it is not reaching here
ETH State in eth handler is (READY STATE --> START STATE)
Error code in eth handler is zero.
Here I have attached my .ioc file
I have updated flash ld file as per repository code
LWIP Debug Messages :
netif: netmask of interface set to 255.255.255.0
netif: GW address of interface set to 192.168.10.10
netif_set_ipaddr: netif address being changed
netif: added interface st IP addr 192.168.10.5 netmask 255.255.255.0 gw 192.168.10.10
netif: setting default interface st
etharp_timer
pbuf_alloced_custom(length=0)
pbuf_alloced_custom(length=0)
pbuf_alloced_custom(length=0)
pbuf_alloced_custom(length=0)
etharp_request: sending ARP request.
pbuf_alloc(length=28)
pbuf_alloc(length=28) == 0x20009804
etharp_raw: sending raw ARP packet.
pbuf_add_header: old 0x20009824 new 0x20009816 (14)
ethernet_output: sending packet 0x20009804
pbuf_free(0x20009804)
pbuf_free: 0x20009804 has ref 1, ending here.
pbuf_free(0x20009804)
pbuf_free: deallocating 0x20009804
pbuf_alloced_custom(length=0)
... after this MCU got stucked.
Solved! Go to Solution.
2025-02-18 2:45 AM
Hello @lavanya ,
unfortunately, there is no support for cmsis V2 FreeRTOS for F7 series.
I have input a ticket (ticket number 203486 for internal reference only) to remove the option for cmsis v2 for FreeRTOS in cube MX.
Regards
2025-02-18 2:45 AM
Hello @lavanya ,
unfortunately, there is no support for cmsis V2 FreeRTOS for F7 series.
I have input a ticket (ticket number 203486 for internal reference only) to remove the option for cmsis v2 for FreeRTOS in cube MX.
Regards
2025-02-26 1:34 AM
Hello @STea
I also tried to update the freerots from V1 to V2 and the run in 1000 of errors when building a working project for an F7. Luckily I found this ticket here after a while!
Is it planed to support the F7 series in the future?
Best regards
CO