2017-11-03 11:25 AM
Hello,
I just wanted to let you know that the stm32cube 4.23 v1.0 generated code for MX_SDIO_SD_Init on the stm32f407 is missing a call to BSP_SD_Init(). BSP_SD_Init is generated by the Cube but never called neither in void MX_SDIO_SD_Init(void) or DSTATUS SD_initialize(BYTE lun). I have attached my ioc file.
I'm generating for VisualGDB (GPDSC).Thank you,
&sharpsdio&sharpfatfs&sharpf407
#stm32f4 #sdio #cube32 #fatfsSolved! Go to Solution.
2018-03-05 5:42 AM
Hello
Ratelle.Charles
,This issue is fixed in CubeMX4.
Please upgrade CubeMX if not already done.
BR. Jeanne
2017-11-05 6:35 AM
You can try this 2 link, until now, I just complete the sd+fatfs mount, open, read, the write, and close still error.
https://community.st.com/0D50X00009XkW2dSAF
https://community.st.com/0D50X00009bMM7JSAW
The CubeMX4.23 + fatfs R0.12 + SD still have many problem to use.
I will change spi+sd+fatfs R0.10 for my application
2017-11-06 12:22 AM
Hello,
This issue is already raised internally to the appropriate team for further review and investigation.
We will come back to you as soon as we have needed details/explanation.
Thanks and Best RegardsImen
2018-03-05 5:42 AM
Hello
Ratelle.Charles
,This issue is fixed in CubeMX4.
Please upgrade CubeMX if not already done.
BR. Jeanne