cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3916-EMVCO UART1 Configuration. I can not configure the UART1 (pins PA11, PA12) to communicate through the USB.

PablodMM
Associate II

I have seen a similar thread for the ST25R3916-DISCO (making appropiate changes in stm32l4xx_hal_msp.c ), however in this board the USB pins are not connected to the same pins and I am not capable of correctly reconnect the solution to PA11, PA12.

UART communication to UART3 (STLINK) works fine.

What am I missing?

Thanks in advance

0 REPLIES 0