cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C0 SDA signal on PC14

rnicolas
Associate II

Hi,

I'm trying to configure pin PC14 to be used as SDA signal as it stated in the datasheets STM32C031C6 and STM32C031G4:

rnicolas_0-1739374796623.png

rnicolas_1-1739374868084.png

To configure the pin (and the the I2C) I am using:

 

 

void SDK_I2C_Init(SDK_I2C_HandleTypeDef *hi2c) {
  LL_I2C_InitTypeDef I2C_InitStruct = {0};
  LL_GPIO_InitTypeDef GPIO_InitStruct = {0};

  LL_RCC_SetI2CClockSource(LL_RCC_I2C1_CLKSOURCE_PCLK1);
  LL_IOP_GRP1_EnableClock(LL_IOP_GRP1_PERIPH_GPIOB);
  LL_IOP_GRP1_EnableClock(LL_IOP_GRP1_PERIPH_GPIOC);
  /**I2C1 GPIO Configuration
  PB8   ------> I2C1_SCL
  PC14   ------> I2C1_SDA
  */
  GPIO_InitStruct.Pin = LL_GPIO_PIN_8;
  GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
  GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
  GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_OPENDRAIN;
  GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
  GPIO_InitStruct.Alternate = LL_GPIO_AF_6;
  LL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = LL_GPIO_PIN_14;
  GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
  GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
  GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_OPENDRAIN;
  GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
  GPIO_InitStruct.Alternate = LL_GPIO_AF_14;
  LL_GPIO_Init(GPIOC, &GPIO_InitStruct);

  LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_I2C1);

  I2C_InitStruct.PeripheralMode = LL_I2C_MODE_I2C;
  I2C_InitStruct.Timing = I2C_TIMING;
  I2C_InitStruct.AnalogFilter = LL_I2C_ANALOGFILTER_ENABLE;
  I2C_InitStruct.DigitalFilter = 2;
  I2C_InitStruct.OwnAddress1 = 180;
  I2C_InitStruct.TypeAcknowledge = LL_I2C_ACK;
  I2C_InitStruct.OwnAddrSize = LL_I2C_OWNADDRESS1_7BIT;
  LL_I2C_Init(I2C1, &I2C_InitStruct);
  LL_I2C_EnableAutoEndMode(I2C1);
  LL_I2C_SetOwnAddress2(I2C1, 0, LL_I2C_OWNADDRESS2_NOMASK);
  LL_I2C_DisableOwnAddress2(I2C1);
  LL_I2C_DisableGeneralCall(I2C1);
  LL_I2C_EnableClockStretching(I2C1);

  LL_I2C_Disable(I2C1);
  LL_I2C_SetTiming(I2C1, I2C_TIMING);
  LL_I2C_Enable(I2C1);
}

 

 

 which is almost the same code that we can find here.

If I configure another pin to work as SDA (PB9 or PB7) the system works perfectly and I can communicate using the I2C protocol.

Is there any configuration that I am missing for that specific pin?

1 ACCEPTED SOLUTION

Accepted Solutions
rnicolas
Associate II

Hey everyone, I just wanted to take a moment to say thank you for all the insights and suggestions!

After hours of debugging, I finally got my I2C communication working with sensor. The issue? A hidden EXTI pin configuration buried in some project files that I wasn't even considering.

I kept reading through my code again and again, and eventually, I realized that the EXTI settings were conflicting with my I2C pinout. Once I removed those calls—boom! Everything started working perfectly.

This was a great reminder that sometimes the problem isn't where you're looking—it’s hiding in plain sight.

Big thanks to everyone who shared their knowledge and helped me troubleshoot this! Your support made all the difference.

View solution in original post

14 REPLIES 14
Andrew Neil
Super User

What board are you running on?

Are you sure that there's no external hardware issues that would prevent PC14 to be used as SDA?

eg, is the pullup present on PC14?

Have you used an oscilloscope to see what, if anything, is happening externally on the pin?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

For the most basic test I'm using the Nucleo-C031C6. The configuration is that one I already sent, and I see if I configure and connect other pins everything works fine, but not PC14. I'm doing the connection with jumper wires. There is nothing else connected between the two components. This setup does not include pull-ups and I rely on the internal pull-ups as described in the pin configuration

For the STM32C031G4 I'm using a propriertary board with 4k7 external pull-ups, and then configuring the pins with 

 

GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;

 

lines are directly connected between the two components, no switching between boards, nothing.

In both cases, PC14 does not seem to work as SDA. 

Again, check that there's no external hardware issues that would prevent PC14 to be used as SDA.

I2C needs pullups - it won't work without them. Internal microcontroller pullups are seldom suitable.

See: https://community.st.com/t5/stm32-mcus-boards-and-hardware/i2c-between-two-nucleo-f446re-boards/m-p/769665/highlight/true#M23992

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil wrote:

Again, check that there's no external hardware issues that would prevent PC14 to be used as SDA.


eg, take look at the User Manual:

AndrewNeil_0-1739378681219.png

https://www.st.com/resource/en/user_manual/um2953-stm32-nucleo64-board-mb1717-stmicroelectronics.pdf#page=18

AndrewNeil_1-1739378737116.png

AndrewNeil_2-1739378786698.png

 

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
KnarfB
Super User

Scan the ref.man. RM0490 Rev 5 for PC14. Especially 4.7.6 FLASH option register (FLASH_OPTR) HSE_NOT_REMAPPED bit. Don't know if this applies to your case.

hth

KnarfB

This does not really apply in the second board that I described, I see from the schematics those are 0 ohm resistors that need to be placed and removed to actually access to PC14 on the pin header and disconnect the LSE. On my second board, there is literally a track that connects the two devices, and no LSE placed on that pin, so my question still stands.

Just checked, I see the value of FLASH_OPTR is 11111111111111111111111010101010, so I can see it is disabled, and still, there is no communication.

TDK
Super User

If you configure PC14 as a GPIO output and toggle it, can you see the waveform on a scope or multimeter? Take the measurement at the SDA pin of the I2C device.

Code seems good. Don't think there's anything else that hasn't been pointed out.

If you feel a post has answered your question, please click "Accept as Solution".

@rnicolas wrote:

Just checked, I see the value of FLASH_OPTR is 11111111111111111111111010101010, so I can see it is disabled, and still, there is no communication.


It is unclear what you mean by no communication? Do you mean you don't see activity using an oscilloscope? 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source