2021-07-05 04:54 AM
Files with error
HAL 1.02.09
stm32f7xx_II_sdmmc.c,
stm32f7xx_mmc.c.
My EMMC 8GB - SANDISK - SDINBDG4-8G-XA
Seems that the ext_csd, used for cards larger than 1GB has a bug.
MX_SDMMC1_MMC_Init() is exiting with an error.
Fix: for now im using HAL 1.02.08, but then cant use more than 1GB of the 8GB EMMC module.
2021-07-07 02:16 AM
Hello @Jørgen Johannessen ,
Welcome to ST Community
The request you have raised will be internally checked and treated accordingly to the priority.
We will give you an update as soon as possible.
Thanks for your contribution.
BeST Regards,
Walid
2021-07-07 02:17 AM
Internal ticket number : 110218
2021-07-09 12:47 AM
Get the error 4 in STM32F7XX_HAL_MMC.C line 2776,
SDMMC_CmdInitTypeDef sdmmc_cmdinit;
uint32_t errorstate;
/* Send CMD9 SEND_CSD */
sdmmc_cmdinit.Argument = Argument;
sdmmc_cmdinit.CmdIndex = SDMMC_CMD_HS_SEND_EXT_CSD;
sdmmc_cmdinit.Response = SDMMC_RESPONSE_SHORT;
sdmmc_cmdinit.WaitForInterrupt = SDMMC_WAIT_NO;
sdmmc_cmdinit.CPSM = SDMMC_CPSM_ENABLE;
(void)SDMMC_SendCommand(SDMMCx, &sdmmc_cmdinit);
/* Check for error conditions */
// errorstate = SDMMC_GetCmdResp1(SDMMCx, SDMMC_CMD_HS_SEND_EXT_CSD,SDMMC_CMDTIMEOUT);
errorstate = 4.
Have tried to change SDMMC_CMDTIMEOUT to 10000, 20000 but still gets the error.
Best regards
Jørgen Johannessen