cancel
Showing results for 
Search instead for 
Did you mean: 

SDIO+eMMC

Posted on June 05, 2012 at 09:10

Hi Andrew,

I work on an application with a STM32F207 and a eMMC memory (THGBM4G8D4GBAIE).

I have some questions for you.

Do you use a file system ? which ? I use the RL-Flash from Keil but it seems to not support sector access. For now, I'm trying FatFS.

The indentification card process is OK, the card answers but I'm not sure about the following commands to retrieve the EXT_CSD or to launch reads/writes (single or multiple blocks). As attached, the traces of the commands with arguments and responses.

Could you check if the order/arguments/responses are corrects ?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0