2024-03-17 11:31 PM
Hello Team,
I have connected the STM32H723ZI2 board to the PC, i could see the virtual drive connection to the PC, but when I use the embedded coder support and generate code and try to flash the board it showing No board connection to the board.
Solved! Go to Solution.
2024-03-18 01:23 AM
The board name would suggest it's a NUCLEO-H743ZI2 with an ST-LINK/V3
2024-03-18 12:08 AM - edited 2024-03-18 05:09 AM
Hello @mvenkat86 ,
What ST-LINK are you using? Try upgrade the ST-Link firmware.
Did you try to use latest release of STM32CubeProgrammer?
Check that the pins are properly connected and make sure that the power supply VDD from the application board is connected to the ST-LINK/V2. (Edit: I mean ST-LINK/V3)
You can share the schematic for further check.
This FAQ may help you: Why my STM32 doesn't start? - STMicroelectronics Community.
2024-03-18 01:23 AM
The board name would suggest it's a NUCLEO-H743ZI2 with an ST-LINK/V3
2024-03-18 10:21 PM
2024-03-19 12:07 AM
So you have a NUCLEO-H723ZG board.
Where's the ZI2 notation coming from? Have you picked the H743ZI2 Target in MATLAB?
2024-03-19 12:13 AM
Hello Tesla,
I have three different boards like H743ZI2, H753ZI and H723ZG, the board with H743and H753 is detecting in matlab for programming, I could not be able to program the H723ZG board.
BR
Venkat
2024-03-19 12:25 AM
So why in the MATLAB HW settings does in indicate H743ZI when you're try to connect to H723ZG ??
Make sure it's associating with the correct board and hardware.
Makes sure you're using most current versions of software and libraries. Work with MATLAB support.
2024-03-19 12:37 AM
2024-03-31 02:22 AM
Have you solved this problem? I can't connect my H743 board to Simulink. Should I use STLink V3?
2024-03-31 05:09 AM
I had some setting issues in linking the matlab with stm32 cube mx ide, this is how the problem solved, I am not sure if it is related to the ST link V3