2023-07-21 4:52 AM - edited 2023-07-24 11:26 PM
Dear Friends,
Edited:
I have a bootloader that I made via I2C through the mailbox of an ST25DV04.
The bootloader works fine, it is able to save in the flash the whole content of the hex file (valid data).
I have added vector table remapping in my "blink" application as indicated in the following post:
https://community.st.com/t5/embedded-software-mcus/how-to-boot-to-random-address-without-vect-tab-offset-stm32f072/m-p/170236#M10247
The problem is that when I go to launch the application the program goes to HardFault_Handler and I can't figure out why.
The code I use to jump into my application:
static void runApp()
{
typedef void (*pFunction)(void);
pFunction Jump_To_Application;
uint32_t JumpAddress;
HAL_I2C_MspDeInit(&hi2c1);
HAL_DeInit();
/* Jump to user application */
JumpAddress = *(__IO uint32_t*) (APP_START + 4);
Jump_To_Application = (pFunction) JumpAddress;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) APP_START);
/* Jump to application */
Jump_To_Application();
}
The content of the flash once the bootloader is executed is the same as if I load my application directly with Cube Ide. I can check this both in Cube Ide and with Cube Programmer.
I would appreciate some help with this issue.
Solved! Go to Solution.
2023-07-24 11:26 PM
Dear administrators, you can delete the post if you want, I finally found the problem.
The problem derived from an erroneous offset in my flashing protocol through the mailbox of st25dv04, it is now solved and works 100%.
2023-07-24 11:26 PM
Dear administrators, you can delete the post if you want, I finally found the problem.
The problem derived from an erroneous offset in my flashing protocol through the mailbox of st25dv04, it is now solved and works 100%.