Flash SR errors on startup
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-09 1:57 AM
Hi all.
I'm working on stm32WB MCU, I have a bootloader and an application. The bootloader only check if any update needed and jump to app. When app stops at main I can see that flash status register is set with PGAERR, SIZERR and PGSERR and I have no idea why it happens. To fix it I added error flags clear on the first flash operation and it works.
I know there are some problems with the second CPU handling ble communication, like the need to clear OPTVERR on startup.
Is there any known problem or am I doind something wrong?
Thanks in advance.
Labels:
- Labels:
-
Flash
0 REPLIES 0