2018-10-21 6:21 AM
I am using soft pulse triggering via "__HAL_TIM_ENABLE(&htim1)" but have a problem with the code shown below.
HAL_TIM_OnePulse_Start(&htim1, TIM_CHANNEL_1);
volatile uint16_t array [300];
HAL_Delay(1000); // let ADC power up
while(1)
{
for(int n=0;n<300;n++) // acquisition loop
{
if (hspi1.State != HAL_SPI_STATE_BUSY_RX)
{
__HAL_TIM_ENABLE(&htim1); //send pulse
HAL_SPI_Receive(&hspi1,(uint8_t*)array[n],1,1); //clock data
HAL_Delay(1);
}
}
}
With the HAL_Delay(1); in the loop, the pulses look fine but for some reason the HAL_SPI_Receive function isn't initiated - there are no clocks. When I remove the delay, the clock is there but the pulse output is almost inverted being high most of the time, and even runs over the receive clock?
I don't quite understand what's going on as I have the != HAL_SPI_STATE_BUSY_RX there but I think it's being ignored?
Thanks
2018-10-21 6:42 AM
I use this for SPI receive:
unsigned char receiveSPI1(unsigned short data) {
char RxSPI;
// Clear_SPI1_nSS_Out();
while (!(hspi1.Instance->SR & SPI_FLAG_TXE)) // Tx buffer is empty ?
;
// is empty now
*((__IO uint8_t *)&hspi1.Instance->DR) = data; // force the SPI to transceive 8 bit
while (!(hspi1.Instance->SR & SPI_FLAG_TXE)) // wait for the transmisson buffer to clear
;
while ((hspi1.Instance->SR & SPI_FLAG_BSY)) // wait for the data to leave the pin
; // here we are loading the Rx buffer
while ((hspi1.Instance->SR & SPI_FLAG_RXNE)) // unload Rxbuffer until its empty
RxSPI = hspi1.Instance->DR;
// Set_SPI1_nSS_Out();
return RxSPI; // the last received byte
}
2018-10-21 6:47 AM
Thanks for the reply, I will bear that in mind.
I am working with others unfamiliar with coding and the rest of the project is using HAL, so we would like to get the HAL working if possible. I am keen to understand what is wrong in my code?
Thanks
2018-10-21 2:57 PM
Timer period lasting longer than the SPI frame?
JW