[NUCLEO-N657X0-Q] ETH1 MAC/DMA not receiving packets & Memory Management Tool problems
- 17 replies
- 668 views
Hello STM32 Community,
I am developing a system on the NUCLEO-N657X0-Q using ThreadX and NetX Duo and I am having a hard time to make the ethernet work. I want to implement a web server in my system but I cannot make the Ethernet communicate.
Problem:
I am unable to receive or transmit any Ethernet frames. The PHY link establishes successfully (from what I see on my linux terminal, autonegotiation completes, Link is UP, and the LEDs on the plug turns on normally), but pinging the Nucleo's static IP yields no response. Wireshark shows no ARP or ICMP packets originating from the Nucleo.
Trying to debug, I see that the the MAC/DMA interrupt `ETH1_IRQHandler` is never triggered by incoming network traffic. It fires exactly twice during the initial board boot sequence(where, for what I understand, some DMA errors flag are raised), but remains completely silent afterward. From the logs that I send to the serial port it appears that from the NetXDuo point of view is everything fine.
The D-cache is disabled and for now I want to keep it disabled, because activating it breaks other parts of my project (I see that in the examples the Dcache is enabled, but I guess is only matters of performance, not mandatory, right?).
Among various attempts, I was also trying to use the Memory Management Tool to move the RAM and FLASH regions in order to assign explicitly regions for the Ethernet descriptors. However, The Tool does not let me move these regions (my project is in XiP mode, if it matters).
I have then some questions about these two related issues:
A) Ethernet and NetX Duo Initialization
1. Am I missing some software initialization step, or misconfiguring the hardware in some way? I went through many examples and I do not find an answer, also given that the configuration sometimes differ among them.
B) Memory Management Tool (XiP Mode)
2. Assuming explicit descriptor placement is necessary for a fix, what is the procedure to unlock, and modify the default memory regions within the STM32CubeMX Memory Management Tool, so that I can define custom memory segments?
Any guidance on resolving the MAC silence or navigating the memory configuration tool would be highly appreciated. Thank you. I attach a .zip file with all the code and the .ioc file.