Migrating project from STM32G474I-eval board to STM32H757I-eval board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-05-29 1:38 AM
Hello,
I'm trying to migrate my project from STM32G474I-eval board to STM32H757I-eval (dual core)' but I'm facing some troubles.
My original project has several peripheral : CANFD, ADC1, DAC, USART. I tried to define all these according to the Data sheet of STM32H757I on Core M7 only (just to try to migrate to single core at the beginning), but when I was trying to check ADC1 I have already encountered some problems.
First of all according to the STMCubeMX the only available pins for ADC1 were (PA0, PA0_C, PA1_C), and in the DMA settings - I put DMA1 Streem3 (Circular). According to data sheet the pin PA0_C is connected to the CN5 and RV1 potentiometer so I was expecting that moving the potentiometer to different values would actually change the output on PA0_C.
The problem is - when I'm running the debugger on the STM32H757I board I always find myself in the HAL_ADC_IRQHandler function, and never get to the ADC_DMAConvCplt callback (where the HAL_ADC_ConvCpltCallback user implemented function is called).
And in the HAL_ADC_IRQHandler the next check fails:
/* ====== Check ADC group regular end of unitary conversion sequence conversions ===== */
if ((((tmp_isr & ADC_FLAG_EOC) == ADC_FLAG_EOC) && ((tmp_ier & ADC_IT_EOC) == ADC_IT_EOC)) ||
(((tmp_isr & ADC_FLAG_EOS) == ADC_FLAG_EOS) && ((tmp_ier & ADC_IT_EOS) == ADC_IT_EOS)))
here the (tmp_isr & ADC_FLAG_EOC) == ADC_FLAG_EOC and
(tmp_isr & ADC_FLAG_EOS) == ADC_FLAG_EOS are TRUE
and the (tmp_ier & ADC_IT_EOC) == ADC_IT_EOC and (tmp_ier & ADC_IT_EOS) == ADC_IT_EOS are FALSE !
Can anyone help me with this ?
Thanks
- Labels:
-
STM32G4 Series
-
STM32H7 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-06-11 3:09 AM
Hello @Ana;
If your initial STM32G474I project is based on STM32CubeMX generation code. I recommend you to look at these articles and get inspired to switch from STM32G474 to STM32H747.
- How to export a project configuration to a compatible STM32
- How to switch from one STM32 to another using STM32CubeMX
Also, I think ADC_DualModeInterleaved example can help you to check the ADC configuration. This example provides a short description of how to use two ADC peripherals to perform conversions in interleaved dual-mode. The data is transferred by DMA.
I hope this help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.