2025-05-28 10:23 PM
PA0_C/PA1_C/PC2_C/PC3_C
What is the base address for the above four GPIOs that can be set?
Also, do you have the following understanding about the above 4 pins?
Pxy_C can be set to a pin of the same function or another function by controlling an analog switch.
Solved! Go to Solution.
2025-05-29 1:13 AM
2025-05-29 1:13 AM
2025-06-11 3:32 AM
Thank you very much.
I understand, there is no separate configuration register for Pxy_C, you are talking about whether or not it is connected via a switch to the Pxy's pins.