2025-08-06 12:42 AM
Hello,
In my project, i am using 2 octoSPI devices connected to my STM32H735. (IDE is STM32CUbeIDE V1.19.0)
After migrating the Project to STM32CubeMX 6.15.0 it is not possible to configure the octoSPI in Multiplexed Mode anymore. The existing config from V6.14.1 and below is automatically removed during the migration and can not be set/activated again.
Is there any issue in this Version or am i missing something?
best regards
Alexander
Solved! Go to Solution.
2025-11-20 8:25 AM
Hello @AZorn.1 ,
Those issues are fixed on the last STM32CubeMX Version.
How to get STM32CubeMX 6.16.0:
Under this link .
Or update your current installation of STM32CubeMX using: Help > Check for Updates
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-06 1:24 AM - edited 2025-08-08 3:43 AM
Hello @AZorn.1 ,
First let me thank you for posting.
The issue of QUADSPI unavailability has been reported in these posts:
STM32CubeIDE 1.19.0 Problem migrating OCTOSPI2 (ST... - STMicroelectronics Community
STM32CUBEIDE Version: 1.19.0 QUADSPI unavailable ... - STMicroelectronics Community
An Internal Ticket was raised to the Development Team ( Ticket Number: 213718 ).
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-06 3:41 AM
Hello Mahmoud,
thank you very much for your reply and the information.
What do you think, when the issue will be fixed, are there any forecasts, or similar available?
best regards
2025-08-06 4:41 AM
Hello @AZorn.1 ,
I will keep you up to date until the issue is solved.
Thanks
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-08 3:58 AM
Hello @AZorn.1 ,
Let me thank you for bringing this issue to our attention (The unavailability of the Multiplexed Mode on STM32CubeMX 6.15).
An Internal Ticket was raised to the Development Team ( Ticket Number: 215540 ).
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-18 9:20 PM
Hello Mahmoud,
i know, you promised to tell us, if there are news according the issue mentioned above. But it is long ago, and i need to ask, how the bugfixing status is.
Please, is there any idea, when a solution can be ready for us?
best Regards
Alexander
2025-11-20 8:25 AM
Hello @AZorn.1 ,
Those issues are fixed on the last STM32CubeMX Version.
How to get STM32CubeMX 6.16.0:
Under this link .
Or update your current installation of STM32CubeMX using: Help > Check for Updates
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-20 10:02 AM
Hello Mahmoud,
Thank you so much, i already updated and it is working again!
best regards