2018-05-21 8:07 AM
I want to use the ETH port to communicate with other devices. I started by creating a project in CubeMX for the STM2F769I-Disc board.
I simply added the LWIP and the ETH port (as RMII) and set a specific IP address (which was not already taken by any other device, my pc included).
I'm using IAR to comile the project and everything is fine: I also added in the while(1) the function MX_LWIP_Process();
My problem is that I don't reach the board at its specific address when I ping it.
Where am I going wrong?
Thank you!
#stm32f7 #lwip #ethSolved! Go to Solution.
2018-05-22 4:59 PM
Make sure you set the PHY address to 0. STM32CubeMX application STILL wants to set it to 1. Come on, ST, how many years do we have to wait?
2018-05-21 11:58 PM
In particular the code returns an error in function HAL_ETH_GetReceivedFrame since the following if statement is not verified:
/* Check if segment is not owned by DMA */
if(((heth->RxDesc->Status & ETH_DMARXDESC_OWN) == (uint32_t)RESET))
What is this statement doing? When is its condition true?
2018-05-22 4:59 PM
Make sure you set the PHY address to 0. STM32CubeMX application STILL wants to set it to 1. Come on, ST, how many years do we have to wait?
2018-05-23 4:39 AM
Thanks for your advice about the PHY parameter! It must have been that. Now it works well!
2018-05-23 5:45 AM
Hello,
The
PHY
address name issue is already fixed in theSTM32CubeMx
4.19 release: You can change the PHY address value in ETH configuration, then go to the 'Parameter Settings' tab.With Regards,
Imen
2018-05-23 6:37 AM
It is NOT fixed in 4.25.1. PHY defaults to 1 - see attached images
2018-05-23 7:06 AM
Hello
doe.john.016
,B
y default,
the PHY address value in ETH configuration is setted to 1, and you can change it to 0.
With Regards,
Imen
2020-03-11 6:53 AM
As far I can see, initially CubeMX starts with the correct PHY address of 0... but then if you (for example) disable and re-enable the ETH device, it changes the PHY address from 0 to 1
We are spending so much time on this stupid CubeMX behaviours...
2023-07-25 5:55 AM
I can't set PHY to 0 because there is no such setting for this card.