cancel
Showing results for 
Search instead for 
Did you mean: 

Library For ST7567 GLCD with STM32G0B1RCT6

Berlin-raj123
Associate III

HI, I am trying to implement ST7567 GLCD (128x64) with SPI on my STM32G0B1RCT6 MCU. Unfortunately i am not getting the Example Driver, i tried my self but there is no improvement, So Any one Kindly send me the STM32 related ST7567 GLCD Example 

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Berlin-raj123 

I modified the example Projects/NUCLEO-G0B1RE/Examples/SPI/SPI_FullDuplex_ComDMA_Master to fit your settings. The SPI sent the data without correctly.

Please find below the used SPI configuration:

static void MX_SPI2_Init(void) { /* USER CODE BEGIN SPI1_Init 0 */ /* USER CODE END SPI1_Init 0 */ /* USER CODE BEGIN SPI2_Init 1 */ /* USER CODE END SPI2_Init 1 */ /* SPI2 parameter configuration*/ hspi2.Instance = SPI2; hspi2.Init.Mode = SPI_MODE_MASTER; hspi2.Init.Direction = SPI_DIRECTION_1LINE; hspi2.Init.DataSize = SPI_DATASIZE_8BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_HIGH; hspi2.Init.CLKPhase = SPI_PHASE_2EDGE; hspi2.Init.NSS = SPI_NSS_SOFT; hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32; hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi2.Init.TIMode = SPI_TIMODE_DISABLE; hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi2.Init.CRCPolynomial = 7; hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE; if (HAL_SPI_Init(&hspi2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SPI2_Init 2 */ /* USER CODE END SPI2_Init 2 */ } void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi) { GPIO_InitTypeDef GPIO_InitStruct = {0}; if(hspi->Instance==SPI2) { /* USER CODE BEGIN SPI2_MspInit 0 */ /* USER CODE END SPI2_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_SPI2_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); /**SPI1 GPIO Configuration PA0 ------> SPI1_SCK PC2 ------> SPI1_MISO PC3 ------> SPI1_MOSI */ GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF1_SPI2; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF0_SPI2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE BEGIN SPI2_MspInit 1 */ /* USER CODE END SPI2_MspInit 1 */ } }
View more

 

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar

View solution in original post

7 REPLIES 7

Perhaps find a developer on your team that can code, or port

Get a scope or logic analyzer on the signals and confirm you have communications,and can interact with the registers, send the initialization sequences.

https://github.com/mithunkamat/ST7567-driver

https://github.com/kaushalparikh/nuttx/blob/master/drivers/lcd/st7567.c

https://www.crystalfontz.com/controllers/Sitronix/ST7567/?srsltid=AfmBOoqNqEOyPlZ8Rv645yC8ZcUo7UJmTZVt-HBAeSso8EuMHTF1lK5u

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Initially, I just wanted to check if the SPI is working, so I used an oscilloscope. I did get a signal, but it looks different than expected. I sent a single data byte, 0xFE, but the oscilloscope on the MOSI pin shows 0x00

here are my connection IOC Connection

Clk = 64 MHZ

mode :Half Duplex Master

Data Size :8 bits

baud rate : 4MBit/S

CPOL : HIGH

CPHASE : 2 EDGE

void Write_Command_SPI(uint8_t cmd) { CS_LOW(); RS_CMD(); // Set RS pin to Command mode HAL_SPI_Transmit(&hspi2, &cmd, 1, HAL_MAX_DELAY); //RS_CMD(); CS_HIGH(); } // Initialize ST7567 void ST7567_Init() { // Reset the display RESET_LOW(); HAL_Delay(50); RESET_HIGH(); HAL_Delay(50); //Send initialization commands // Example initialization commands, consult ST7567 datasheet for details Write_Command_SPI(0xAE); // Display OFF Write_Command_SPI(0xA2); // Set Bias Write_Command_SPI(0xA0); // Set SEG Direction Write_Command_SPI(0xC8); // Set COM Direction Write_Command_SPI(0xA4); // Disable Entire Display ON Write_Command_SPI(0xA6); // Normal Display Write_Command_SPI(0x2F); // Power Control Write_Command_SPI(0x27); // Set Contrast Write_Command_SPI(0x81); // Set Electronic Volume Write_Command_SPI(0x10); // Set Volume Write_Command_SPI(0xAF); // Display ON } main() { MX_SPI2_Init(); /* USER CODE BEGIN 2 */ // Initialize the ST7567 display //ST7567_Init(); /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ // Send test data periodically for SPI signal check Write_Command_SPI(0xFE); HAL_Delay(100); // Wait 100ms to easily observe SPI signals on CRO }
View more

 

how to get the single data?WhatsApp Image 2024-11-07 at 7.14.51 PM.jpeg

Connect the probe to MOSI. Currently it looks like it's connected to SCK.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

no dude! i connected everything correctly

I verified hardware connection, as per our connection set up,

Controller - SPI2 CLK is connected to CRO channel1 SCK

Controller - SPI2 MOSI is connected to CRO channel3 MOSI 

Controller - SPI2 CS is connected to CRO channel4 CS

Anyone please help me!! i am waiting for your response

Hello @Berlin-raj123 

I modified the example Projects/NUCLEO-G0B1RE/Examples/SPI/SPI_FullDuplex_ComDMA_Master to fit your settings. The SPI sent the data without correctly.

Please find below the used SPI configuration:

static void MX_SPI2_Init(void) { /* USER CODE BEGIN SPI1_Init 0 */ /* USER CODE END SPI1_Init 0 */ /* USER CODE BEGIN SPI2_Init 1 */ /* USER CODE END SPI2_Init 1 */ /* SPI2 parameter configuration*/ hspi2.Instance = SPI2; hspi2.Init.Mode = SPI_MODE_MASTER; hspi2.Init.Direction = SPI_DIRECTION_1LINE; hspi2.Init.DataSize = SPI_DATASIZE_8BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_HIGH; hspi2.Init.CLKPhase = SPI_PHASE_2EDGE; hspi2.Init.NSS = SPI_NSS_SOFT; hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32; hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi2.Init.TIMode = SPI_TIMODE_DISABLE; hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi2.Init.CRCPolynomial = 7; hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE; if (HAL_SPI_Init(&hspi2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SPI2_Init 2 */ /* USER CODE END SPI2_Init 2 */ } void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi) { GPIO_InitTypeDef GPIO_InitStruct = {0}; if(hspi->Instance==SPI2) { /* USER CODE BEGIN SPI2_MspInit 0 */ /* USER CODE END SPI2_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_SPI2_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); /**SPI1 GPIO Configuration PA0 ------> SPI1_SCK PC2 ------> SPI1_MISO PC3 ------> SPI1_MOSI */ GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF1_SPI2; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF0_SPI2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE BEGIN SPI2_MspInit 1 */ /* USER CODE END SPI2_MspInit 1 */ } }
View more

 

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar