2024-08-07 7:14 AM
Hi,
I am trying to use the DTS on the STM32H5, but after i call HAL_DTS_Start_IT(&hdts), the state of the handle is stuck in HAL_DTS_STATE_BUSY, resulting in a HAL_BUSY when i am trying to get the temperature via HAL_DTS_GetTemperature(&hdts, &temperature) in the HAL_DTS_EndCallback(DTS_HandleTypeDef *hdts).
I debugged through my code and the HAL library and found out that during the execution of the HAL_DTS_Start_IT(&hdts) code (see below) it jumps directly into the HAL_DTS_EndCallback(DTS_HandleTypeDef *hdts) after Line 47 and therefore never reaches Line 50, where the handle state would be set back to HAL_DTS_STATE_READY.
I "fixed" this problem for now by either setting the state manually back to HAL_DTS_STATE_READY at the beginning of the HAL_DTS_EndCallback(DTS_HandleTypeDef *hdts) or commenting out the HAL_Delay(TS_TIMEOUT_MS) call in Line 47.
My DTS_HandleTypeDef configuration is:
DTS_HandleTypeDef hdts = {.Instance = DTS,
.Init = {.QuickMeasure = DTS_QUICKMEAS_DISABLE,
.RefClock = DTS_REFCLKSEL_PCLK,
.TriggerInput = DTS_TRIGGER_HW_NONE,
.SamplingTime = DTS_SMP_TIME_15_CYCLE,
.Divider = 250,
.HighThreshold = 100,
.LowThreshold = 0}};
and the frequency of my clock is 250MHz.
Does anybody have another "cleaner" solution for this? or might this be a bug of the HAL-Library itself?
Thanks in advance.
HAL_StatusTypeDef HAL_DTS_Start_IT(DTS_HandleTypeDef *hdts)
{
uint32_t Ref_Time;
/* Check the DTS handle allocation */
if (hdts == NULL)
{
return HAL_ERROR;
}
if (hdts->State == HAL_DTS_STATE_READY)
{
hdts->State = HAL_DTS_STATE_BUSY;
/* On Asynchronous mode enable the asynchronous IT */
if (hdts->Init.RefClock == DTS_REFCLKSEL_LSE)
{
__HAL_DTS_ENABLE_IT(hdts, DTS_IT_TS1_AITE | DTS_IT_TS1_AITL | DTS_IT_TS1_AITH);
}
else
{
/* Enable the IT(s) */
__HAL_DTS_ENABLE_IT(hdts, DTS_IT_TS1_ITE | DTS_IT_TS1_ITL | DTS_IT_TS1_ITH);
}
/* Enable the selected DTS sensor */
__HAL_DTS_ENABLE(hdts);
/* Get Start Tick*/
Ref_Time = HAL_GetTick();
/* Wait till TS1_RDY flag is set */
while (__HAL_DTS_GET_FLAG(hdts, DTS_FLAG_TS1_RDY) == RESET)
{
if ((HAL_GetTick() - Ref_Time) > DTS_DELAY_STARTUP)
{
return HAL_TIMEOUT;
}
}
if (__HAL_DTS_GET_TRIGGER(hdts) == DTS_TRIGGER_HW_NONE)
{
/* Start continuous measures */
SET_BIT(hdts->Instance->CFGR1, DTS_CFGR1_TS1_START);
/* Ensure start is taken into account */
HAL_Delay(TS_TIMEOUT_MS);
}
hdts->State = HAL_DTS_STATE_READY;
}
else
{
return HAL_BUSY;
}
return HAL_OK;
}
2024-08-08 4:30 AM
Hi @luc1 ,
Unfortunately the example provided in STM32CubeH5 firmware package is based on polling mode not interrupt mode.
My recommendations in your case:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.