2024-01-16 5:11 PM
Hi Folks,
I'd like to find an example of accessing a USB drive using the STM32CubeIDE. I'm currently using the Nucleo-H7A3Zi-Q board.
I believe I have setup the hardware correctly using the device configuration tool but I can't seem to find a simple or concise example on how to develop the code.
I have downloaded the STM32Cube_FW_H7_V1.11.0 code and examples but it still seems more complicated than it should. I've looked at STM32Cube_FW_H7_V1.11.0\Projects\NUCLEO-H7A3ZI-Q\Applications\USB_Host\MSC_Standalone\ but I don't understand how (or what) to import into my workspace.
For a start I just want to be able to write a "Hello World" into a file on the USB key.
Anybody have a good tutorial or example I can use?
Thanks,
Richard
2024-01-19 2:10 PM - edited 2024-01-19 2:12 PM
Now you have a working drive - so standard fat commands are your friends now...
read from master Chan:
http://elm-chan.org/fsw/ff/00index_e.html
+ examples...
look here:
https://evenlund.blogspot.com/2016/10/usb-storage-with-stm32f4-discovery-and_58.html
/* Create and Open a new text file object with write access */
if(f_open(&MyFile, "Even.TXT", FA_CREATE_ALWAYS | FA_WRITE) != FR_OK)
{
/* 'STM32.TXT' file Open for write Error */
USB_Error_Handler();
}
else
{
/* Write data to the text file */
res = f_write(&MyFile, wtext, sizeof(wtext), (void *)&byteswritten);
if((byteswritten == 0) || (res != FR_OK))
{
/* 'STM32.TXT' file Write or EOF Error */
USB_Error_Handler();
}
else
{
/* Close the open text file */
f_close(&MyFile);
/* Open the text file object with read access */
if(f_open(&MyFile, "Even.TXT", FA_READ) != FR_OK)
{
/* 'STM32.TXT' file Open for read Error */
USB_Error_Handler();
}
else
{
/* Read data from the text file */
res = f_read(&MyFile, rtext, sizeof(rtext), (void *)&bytesread);
if((bytesread == 0) || (res != FR_OK))
{
/* 'STM32.TXT' file Read or EOF Error */
USB_Error_Handler();
}
else
{
/* Close the open text file */
f_close(&MyFile);
--- BUT dont this in endless loop , only one time. :)
2024-01-21 1:00 PM
I got it reading and writing to the USB drive. At least with the small text sample from the code above. But that brings up another question - the sample code was able to create a text file named "Even.TXT" that contains the proper text "This is STM32 working with FatFs" but the file doesn't have a Date Modified value. There is no date or time associated with the file. How do I get a date and time for the file?
How would you write a 1Kb text file to the USB drive? Would you write chunks of data?
Thanks again,
Richard
2024-01-21 1:49 PM
Good ! :thumbs_up:
> There is no date or time
I dont know - you have RTC running, with actual date on your system ? (How it should know it otherwise ?)
see cube :
+
>How would you write a 1Kb text file to the USB drive?
open file, as in example, then write the kB , then close file.
/*-----------------------------------------------------------------------*/
/* Write File */
/*-----------------------------------------------------------------------*/
FRESULT f_write (
FIL* fp, /* Pointer to the file object */
const void* buff, /* Pointer to the data to be written */
UINT btw, /* Number of bytes to write */
UINT* bw /* Pointer to number of bytes written */
)
{
2024-01-22 12:40 PM
I got the timestamp to work. I had the proper settings in the IOC file but it still wasn't working. I looked around and found a variable in ffconf.h that needed to be set to 1. Line 220 = #define _FS_NORTC 1. It was set to zero. Now I am getting the file created with the time stamp.
2024-01-22 2:26 PM
Actually it's not working correctly. Turns out setting FS_NORTC = 1 bypasses the RTC and uses values set in the ffconf.h file.
I need to figure out how to use the
get_fattime();