2020-04-27 9:00 AM
Is there a bug in the SVD file for the STM32G431? It appears to list ADC12_Common->CCR as being at address 0x50000208 when it supposed to be at 0x50000308
2020-04-27 9:42 AM
Hello @frank ,
This issue is already detected and under resolution
Regards
2020-04-28 3:35 AM
Can you also please check the CPAC and SCB definitions.
2020-04-28 5:51 AM
Hi @frank ,
Please note that the SCB iissue i reported internally, following this request: https://community.st.com/s/question/0D53W000004IkPuSAK/most-up-to-date-svd-for-stm32g474.
For CPACR and ADC_COMMON base addresses: they are already fixed in internal version of SVD files that will be available soon on the web and deployed for the IDEs.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.