cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to use SPI interface for Ethernet 100Mbps? STM32H75X device.

MK.111
Associate II

Is it possible to use SPI interface for Ethernet 100Mbps?

Please provide the required configurations/manuals if any. Thanks

5 REPLIES 5
TDK
Guru

No.

If you feel a post has answered your question, please click "Accept as Solution".
MK.111
Associate II

Hi TDK,

Thank you for your quick inputs.

Actually I meant Ethernet over SPI interface, any related information/suggestions of PHY Dev's and it's driver support on STM32H755.

-Thanks​

Probably best not to have multiple concurrent threads on the same theme/design

https://community.st.com/s/question/0D53W000011WyEGSA0/ethernet-design-requirement-with-stm32h755

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Obviously if you have a chip with an SPI interface, that then drives the ethernet, like the Wiznet chips, that is possible.
If you feel a post has answered your question, please click "Accept as Solution".
MK.111
Associate II

Thank you TDK for your answers.

Sure Tesla DeLorean, We can close this thread. I'm unable to find an option 'close thread'. Thanks