User Activity

Dear Experts,I would like to start with the STM32H755 device, which shall have the interfaces,EthernetEthernet over SPIMay I have your inputs on identifying the eval board, Ethernet to SPI adapter card to start with?Thanks
Dear Experts,We have a design requirement with STM32H755 to work with Parallel Redundancy Protocol (PRP). Any relevant help or sources available.Thanks in advance.
Dear Experts,We have a design with STM32H755 having 3 Ethernet ports. Out of which 1 is over RMII controller the other two are over SPI interface.My queries are as follows,1. We want to run all 3 three Ethernets at the same time, How to handle this s...
Is it possible to use SPI interface for Ethernet 100Mbps?Please provide the required configurations/manuals if any. Thanks
Is it possible to use GPIO interface to work with MIL1553B HI-6130PQTF chipset?Please provide the configuration settings for the same. Thanks