2021-06-01 1:36 AM
Hello,
I want to use ADC1 with 5 Channels, ADC2 with 2 Channels and ADC3 with 1 Channel.
I configured everything for triple Mode. After I started ADC2 and ADC3 do I start ADC1 like this.
Is NUMBER_OF_CHANNELS supposed to be 8 in my case?
retVal = HAL_ADCEx_MultiModeStart_DMA(&hadc1, gValueArrayADCTripleMode, NUMBER_OF_CHANNELS);
I test the output by looking at ADC1 Channel7, but the index of this value changes every conversion. How can I get every value to stay at the same position in the array? The values itself seem to be valid. I just can figure the positioning out.
2021-06-01 6:02 AM
I think I found the answer. If ADC1 has 5 Channels ADC2 and ADC3 also need to have 5 Channels. Can anyone confirm?