2023-01-20 2:28 AM
Hello,
I am using STM32L4q52gt6P controller. for application development, I am using freeRTOS.
When no task running in RTOS at that time I put the controller in sleep mode from the idea task of RTOS.
I have used 12Mhz of HSE, 16Mhz-SYSCLK with PLLCK, AHB Prescaler -1, HCLK 16Mhz, and most of the GPIO are used.
Also, I am using external SMPS for VDD1V2.
My MCU current Consumption is around 3.24mA in run mode and 1.2mA in Sleep mode.
I have added a snap of the datasheet STM32_RUN_MODE
I want MCU current consumption as per mentioned for fHCLK 16Mhz in the datasheet.
Anyone, please suggest to me what thing I need to set to achieve 0.88 mA current of CPU?
What are the steps I need to take care to achieve this or where I need to debug or which additional HAL API needs to config 0.88 mA current of CPU?
Your response will be highly appreciable to me
2023-01-20 3:03 AM
Hello @BGajj.1 ,
Did you set all free pins as analog ? as it helps reducing the consumption
Please check this article
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-20 3:25 AM
Hello @Sarra.S,
Thanks for you response!
20 GPIO pins out of 144 pins I am not using. And yea I have keep those 20 pins as analog.
Is it okay to just keep those pins as analog or i need to disable the clock for those pins?
2023-01-20 12:44 PM
Read at least the section 3 of this article: