cancel
Showing results for 
Search instead for 
Did you mean: 

Hello! I am getting constant ADC value through SPI when I add a debug message using UART on STM32F205 with CMSIS RTOS.

TBhil.1
Associate II

We have interfaced CS5532 using SPI which is initialized in continuous conversion mode. We read the ADC count in a task being called every 160 ms. When I add following statements in the task, the ADC count read from CS5532 becomes constant.

sprintf(Debug,",%ld,%f,%d\n\r",ADC_Sum,CurrentWt,StableFlag);

uart0Puts(Debug);

Removing above code solves the problem. I have also noticed that adding/removing similar debug messages in/from other parts of code also creates same problem. I commented similar statements from a function that is not getting called with current settings in EEPROM. This also caused same problem. The code works fine when no such debug message is used. I also checked the stack usage using ST Link debugger and found it to be within limits. Any kind insights on how to approach this problem would really be helpful. Thank you.

2 REPLIES 2
Karl Yamashita
Principal

You need to post your uart0Puts function and any other functions it may call. Post what is in the task as well.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
TBhil.1
Associate II

The code is as follows:

void Timer0_Procedure(void const *arg)// __task

{

Timer0_Th_Id = osThreadGetId();

Timer_Sem = osSemaphoreCreate(osSemaphore(Timer_Sem), 0);

while(1)

{

osSemaphoreWait(Timer_Sem, osWaitForever);

// if(Timer0Event.status == osEventSignal)

{

AdcReadCounter++;

if(AdcReadCounter == 2) //160ms -> 6.25 SPS

{

AdcReadCounter = 0;

ADC_DATA = CS5532_Read_ADC(); // read ADC data

// sprintf(Debug, "%ld\r\n", ADC_DATA);

// uart0Puts(Debug);

osSignalSet(tsk1,0x0002);//isr_evt_set (0x0002,tsk1); // event set for processing ADC data

}

c160_counter++;

c160_ADC=1;

Global_80ms=1;

if(std_cal_stable_counter != 0xFFFF) //counter increment moved in ISR in order to solve std cal getting aborted after Lin 9 issue

{

if(StableFlag)

std_cal_stable_counter++;

else

std_cal_stable_counter = 0;

}

if(c160_counter==2)   //if part added by RAHUL to sync with 160ms timing

{

LCM_Display_Flag = 1; // set LCM display flag

autocal_timer++;

AutoOff_timer++;

c160_counter =0;

iStability_Density_Counter++;   //added by rahul

if(iStability_Density_Counter>=282)   // 282 to 141

{

cStability_time_den=1;

iStability_Density_Counter=0;

}  //end added by rahul

}

if (Cal_trigger_time || cal_temp_trigger || cal_trigger_after15min || cal_trigger_after5_20min)

{

cIntCal_counter++;

}

if (Start_15min_Counter == 1)

{

cIntCal_15min_counter++;

if (cIntCal_15min_counter >= INTCAL_AFTER_SUCESSFUL_CAL)

{

cal_trigger_after15min = 1;

LCM_DisplaySymbol(LCM_CODE_INCAL);

cIntCal_15min_counter = 0;

}

}

if(Autocal_Enable==1)

{

if (Start_Five_Twenty_Min_Counter==1)

{

Intcal_After_5min_20min++;

}

if (Intcal_After_5min_20min >= Intcal_5Min20Min_Band)

{

cal_trigger_after5_20min=1;

}

if ((Intcal_After_5min_20min>=18750)||(Cal_trigger_time)||(cal_temp_trigger)||(cal_trigger_after15min))// temp cahnged for testing  //18750 25 min

{

Intcal_5Min20Min_Band = 0;

Start_Five_Twenty_Min_Counter=0;

Intcal_After_5min_20min=0;

// cal_trigger_after5_20min=0;

Perform_5min_20min_Intcal=0;

}

}

if(QMS_Page2r_Send)

{

QMS_Page2r();

QMS_Page2r_Send = 0;

}

if(QMS_Unstable_ADC_Weight_Temp)

{

sprintf(Debug,"&A:%ld&W:%lf&T:%0.3lf&S:%d\r\n",ADC_Sum,Simple_Weighing_Weight,Current_Temp,StableFlag);

uart0Puts(Debug);

}

if(QMS_MdNo_SrNo_Send)

{

  QMS_MdNo_SrNo_Send = 0;

  QMS_MdNo_SrNo();

}

}

}

}

This is a task in which ADC read function is called. The semaphore in this task is released from a timer ISR after every 80 ms. ADC is being read every 160 ms. ADC_Data_Process task is activated after this.

void ADC_Data_Process(void)

{

//---------------------added by rahul------------------------------------------------

ADC_RECORD *ptrAdcRecord ; //Poonam

osMutexWait(ADC_Protect_id, osWaitForever);//os_mut_wait (ADC_Protect, 0xffff);

//---------------------new vibration algo------------------------------------------------

 ptrAdcRecord = validate(ADC_DATA);  //its on in backgroud

  if(SWM_Dosing==TRUE)

ptrAdcRecord->mSummedAdc = getSummedAdc(ptrAdcRecord->mRawAdc); //ADC value After Noise Elimination

else

 ptrAdcRecord->mSummedAdc = getSummedAdc(ADC_DATA); //Noise Elimination Excluded ADC value

getAverage(ptrAdcRecord, StableFlag);

ADC_Sum = ptrAdcRecord->mAvgAdc;

sprintf(Debug,",%ld,%f,%d\n\r",ADC_Sum,CurrentWt,StableFlag);

uart0Puts(Debug);

//------------------------------------------------------stability----------------------------------------------------------------------

if(CheckStability(ADC_Sum))  //was 49, changed by rahul

{

StableFlag = 1;  // stable flag set

cCreep_Counter++;

if(cCreep_Counter >= NINE_SEC) //TEN_SEC =10000/80= 125 counts 112

{   

cEnter_Creep = 1;

cCreep_Counter = NINE_SEC; //after 9 second stable mark it enters here

}

else

{

StableFlag=0;

cCreep_Counter=0;

cEnter_Creep=0;

cSaved_Wt_Flag=0;

cCreep_Done = 0;

if( fabs(Creep_Weight) < (WeighingAccuracy_Local*2)) //creep weight is less than 0.0002

{

Creep_Weight = 0;  //make creep weight zero

previous_weight_Accumulated_Creep = 0;

now_Creep_Weight = 0;

}

else

  {

previous_weight_Accumulated_Creep = 1;

if(yes_in)

{

if( fabs(now_Creep_Weight) < (WeighingAccuracy_Local*2))

{

Creep_Weight = Creep_Weight - now_Creep_Weight;

//now_Creep_Weight = 0;

}

else

;//previous_weight_Accumulated_Creep = 1;

yes_in=0;

now_Creep_Weight = 0;

}

}

}

Temp_Read_Count++;

if(Temp_Read_Count >= 2)

{

osSignalSet(tsk2, 0x0004);//os_evt_set (0x0004,tsk2); // for temperature read event set after 2 ADC data

Temp_Read_Count = 0;

// Read_Temp = 1;

osMutexRelease(ADC_Protect_id);//os_mut_release (ADC_Protect);   // mutex released

void uart0Puts(const char *string)

{

char ch;

const char *dummy_string;

if(!Feature_Setting.printer_Set) // for Printer settings

{

return;

}

if(PrinterState == PRINTSTATE_OFF)

return; 

osSemaphoreWait(semaphore1, osWaitForever);//os_sem_wait (semaphore1, 0xffff); // wait for semaphore indefinite

dummy_string = string;

while ((ch = *dummy_string)!=0)

{

if (putchr(ch)<=NULL_CHARACTER) break; // check end of string

if ((ch == '\n' || ch == '\r') && (cWinPrint_Enable == 1)) break; //anup windows

dummy_string++;

}

osSemaphoreRelease(semaphore1);//os_sem_send (semaphore1); // release semaphore

}

unsigned char putchr (unsigned char ch) 

{

while(!(USART_GetFlagStatus(USART3, USART_FLAG_TXE)));

USART_SendData(DEBUG_USART,ch);

return 1;//(USART3->DR = (ch & (uint16_t)0x01FF));

}